This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSV4 is not connecting with TMS320F2812 ( XDS100 V1 USB EMULATOR)



Sir,

    Am using TMS320F2812 kit ( XDS100 USB EMULATOR ) with Code Composer Studio V 4.1.0.02006. After Successful build , when am trying to connect ( Target - Connect target ) the target. am getting following Errors;

1. Error connecting to the target:
Error 0x00001200/-1135
Error during: OCS, Target,
Unrecoverable emulation error

if i retry then i get following error :

2. Error connecting to the target:
Error 0x00001200/-1041
Error during: OCS, Target,
Device driver: Problem with the Emulation Controller.
It is recommended to RESET EMULATOR.  This will disconnect each
target from the emulator.  The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.

then i give cancel.. , Continue launching -- Yes . then reset emulator , then terminate all............. once again i started the from the beginning the same response at all times.

Notes For your referrence:

1. I monitor the 1.8v and 3.3v while target connect. it constant at respective voltage. no lag or lead in voltages . 

2. am using 25 Mhz crystal ., and i  checked . once i power the kit it producing the 25 Mhz clock with 168mv peak to peak.

3. I uninstall the code composer studio and reinstalled,,,, yet same response.

4. My reset pin automatically  keep on Getting low for 20us . according to datasheet : " Device Reset (in) and Watchdog Reset (out).
Device reset. XRS causes the device to
terminate execution. The PC will point to the
address contained at the location 0x3FFFC0.
When XRS is brought to a high level,
execution begins at the location pointed to by
the PC. This pin is driven low by the DSP when a watchdog reset occurs. During
watchdog reset, the XRS pin will be driven low
for the watchdog reset duration of
512 XCLKIN cycles.
The output buffer of this pin is an open-drain
with an internal pullup (100 µA, typical). It is
recommended that this pin be driven by an
open-drain device. "

I think watchdog timer keeps on resetting , hence this pin goes low for periodically . ........ if my thinking is correct  please tell me how to stop the WATCHDOG TIMER before start programming the target ..

and my one more doubt is " May be for processor failure this response is showing  "  Please Kindly help me to solve this issue ..

Many Thanks,

Thiyagarajan.S

  • Thiyagarajan,

    Although I am not an expert in hardware (you seem to have verified some of the important topics), I strongly recommend going through the debugging strategy of the page below:

    http://processors.wiki.ti.com/index.php/Debugging_JTAG_Connectivity_Problems 

    The watchdog is something that will cause a reset on the device, but I don't think it would case the unrecoverable emulation error you see... This seems more consistent with either a failure between the PC and the emulator or a misconfiguration (XDS100v1 versus v2, etc.)

    One more detail: if this is a custom board, check if the same error message can be reproduced in a F2812 development kit - this will rule out any problems with either the hardware or the software configuration. 

    Hope this helps,

    Rafael

  • HI desouza,

        okay i will take care of hardware , Kindly tell me about CCS ., For what kind possible issues i may get this errors ...Please

    Many Thanks,

    Thiyagarajan.S

  • Thiyagarajan,

    desouza said:

    The watchdog is something that will cause a reset on the device, but I don't think it would case the unrecoverable emulation error you see... This seems more consistent with either a failure between the PC and the emulator or a misconfiguration (XDS100v1 versus v2, etc.)

    Also, did you check the page I sent before? There it talks about several tips and contains information about the utility we use to debug these scenarios.

    Regards,

    Rafael