This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Debug processor selection in multiprocessor environment with CCS4

Other Parts Discussed in Thread: TMS320F28066

I had setup multiprocessor environment with two TMS320F28066 devices and using CCS  4.2.3.00004

Using Signum JTAGJetC2000

I could able to configure, connect and Flash programs into individual DSPs without any trouble. But I could not able to debug them.

Regardless of what device I clicked, it loads the debug program in to only first device in the daisy chain.

If i select first device for debug, the debug operation is fine.

If i select second device and click debug, it tries to load but the debug doesn't happen.

Can anyone confirm that, whether I can select any device and debug them independently in the multiprocessor environment.