Other Parts Discussed in Thread: TMS320C6678
I have bought the TMDXEVM6678L EVM and installed all software from the accompanying disk, and followed the attached readme files and installation guides.
I have imported the hua project into my workspace, and tries to make contact with the evm hardware via the Blackhawk XDS560v2-USB Mezzanine Emulator.
From the Target Configuration tab, double click the My6678hua.ccxml and sees that the configuration looks ok.The I press the underlined "Target Configuration" text, and get an overview over the configuration. The root has name "Blackhawk XDS560v2-USB Mezzanine Emulator_0". Next branch is named TMS320C6678_0. Then Icepick-D, and 8 subpaths, one for each CPU kernel lies underneath. If select a CPU and press the "Test Configuration" button, the test runs mostly as expected. The output is shown in an attached file.
However, maybe one out of 3 times, the test stops after line "Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc", and CCS is frozen.
I am also trying to launch the configuration:
From the Target Configuration tab, i right-click the My6678hua.ccxml file and selects "Launch Selected Configuration". Again, about of 1 of 3 trials leads to CCS freezed.
If I, after a successful "Launch Selected Configuration" selects a CPU in the Debug tab and tries "Run->Connect target", CCS most often freeze telling "Executing Connect Target". A few times it passes this phase also, but e. g. trying to view CPU registers leads to CSS freezed again.
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\Users\oddt\AppData\Local\.TI\213602635\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'bh560v2u.out'.
Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc
The library build date was 'Aug 30 2012'.
The library build time was '22:16:38'.
The library package version is '5.0.838.0'.
The library component version is '35.34.40.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '5' (0x00000005).
The controller has an insertion length of '0' (0x00000000).
The cable+pod has a version number of '8' (0x00000008).
The cable+pod has a capability number of '7423' (0x00001cff).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.
-----[Print the reset-command hardware log-file]-----------------------------
The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the Nano-TBC VHDL.
The link is a 560-class second-generation-560 cable.
The software is configured for Nano-TBC VHDL features.
The controller will be software reset via its registers.
The controller has a logic ONE on its EMU[0] input pin.
The controller has a logic ONE on its EMU[1] input pin.
The controller will use falling-edge timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '2' (0x0002).
The utility logic has not previously detected a power-loss.
The utility logic is not currently detecting a power-loss.
Loaded FPGA Image: C:\ti\ccsv5\ccs_base\common\uscif\dtc_top.jbc
-----[The log-file for the JTAG TCLK output generated from the PLL]----------
Test Size Coord MHz Flag Result Description
~~~~ ~~~~ ~~~~~~~ ~~~~~~~~ ~~~~ ~~~~~~~~~~~ ~~~~~~~~~~~~~~~~~~~
1 none - 01 00 500.0kHz - similar isit internal clock
2 none - 01 09 570.3kHz - similar isit internal clock
3 512 - 01 00 500.0kHz O good value measure path length
4 128 - 01 00 500.0kHz O good value auto step initial
5 128 - 01 0D 601.6kHz O good value auto step delta
6 128 - 01 1C 718.8kHz O good value auto step delta
7 128 - 01 2E 859.4kHz O good value auto step delta
8 128 + 00 02 1.031MHz O good value auto step delta
9 128 + 00 0F 1.234MHz O good value auto step delta
10 128 + 00 1F 1.484MHz O good value auto step delta
11 128 + 00 32 1.781MHz O good value auto step delta
12 128 + 01 04 2.125MHz O good value auto step delta
13 128 + 01 11 2.531MHz O good value auto step delta
14 128 + 01 21 3.031MHz O good value auto step delta
15 128 + 01 34 3.625MHz O good value auto step delta
16 128 + 02 05 4.313MHz O good value auto step delta
17 128 + 02 13 5.188MHz O good value auto step delta
18 128 + 02 23 6.188MHz O good value auto step delta
19 128 + 02 37 7.438MHz O good value auto step delta
20 128 + 03 07 8.875MHz O good value auto step delta
21 128 + 03 15 10.63MHz O good value auto step delta
22 128 + 03 1E 11.75MHz {O} good value auto step delta
23 512 + 02 3E 7.875MHz O good value auto power initial
24 512 + 03 0E 9.750MHz O good value auto power delta
25 512 + 03 16 10.75MHz O good value auto power delta
26 512 + 03 1A 11.25MHz O good value auto power delta
27 512 + 03 1C 11.50MHz O good value auto power delta
28 512 + 03 1D 11.63MHz O good value auto power delta
29 512 + 03 1D 11.63MHz O good value auto power delta
30 512 + 03 13 10.38MHz {O} good value auto margin initial
The first internal/external clock test resuts are:
The expect frequency was 500000Hz.
The actual frequency was 499110Hz.
The delta frequency was 890Hz.
The second internal/external clock test resuts are:
The expect frequency was 570312Hz.
The actual frequency was 569976Hz.
The delta frequency was 336Hz.
In the scan-path tests:
The test length was 16384 bits.
The JTAG IR length was 6 bits.
The JTAG DR length was 1 bits.
The IR/DR scan-path tests used 30 frequencies.
The IR/DR scan-path tests used 500.0kHz as the initial frequency.
The IR/DR scan-path tests used 11.75MHz as the highest frequency.
The IR/DR scan-path tests used 10.38MHz as the final frequency.
-----[Measure the source and frequency of the final JTAG TCLKR input]--------
The frequency of the JTAG TCLKR input is measured as 10.37MHz.
The frequency of the JTAG TCLKR input and TCLKO output signals are similar.
The target system likely uses the TCLKO output from the emulator PLL.
-----[Perform the standard path-length test on the JTAG IR and DR]-----------
This path-length test uses blocks of 512 32-bit words.
The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 6 bits.
The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.
-----[Perform the Integrity scan-test on the JTAG IR]------------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG IR Integrity scan-test has succeeded.
-----[Perform the Integrity scan-test on the JTAG DR]------------------------
This test will use blocks of 512 32-bit words.
This test will be applied just once.
Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.
The JTAG DR Integrity scan-test has succeeded.
[End]
<?xml version="1.0" encoding="UTF-8" standalone="no"?>
<configurations XML_version="1.2" id="configurations_0">
<configuration XML_version="1.2" id="Blackhawk XDS560v2-USB Mezzanine Emulator_0">
<instance XML_version="1.2" desc="Blackhawk XDS560v2-USB Mezzanine Emulator_0" href="connections/BH-XDS560v2-USB_Mezzanine.xml" id="Blackhawk XDS560v2-USB Mezzanine Emulator_0" xml="BH-XDS560v2-USB_Mezzanine.xml" xmlpath="connections"/>
<connection XML_version="1.2" id="Blackhawk XDS560v2-USB Mezzanine Emulator_0">
<instance XML_version="1.2" href="drivers/tixds560icepick_d.xml" id="drivers" xml="tixds560icepick_d.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds560c66xx.xml" id="drivers" xml="tixds560c66xx.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds560cs_dap.xml" id="drivers" xml="tixds560cs_dap.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds560csstm.xml" id="drivers" xml="tixds560csstm.xml" xmlpath="drivers"/>
<instance XML_version="1.2" href="drivers/tixds560etbcs.xml" id="drivers" xml="tixds560etbcs.xml" xmlpath="drivers"/>
<platform XML_version="1.2" id="platform_0">
<instance XML_version="1.2" desc="TMS320C6678_0" href="devices/C6678.xml" id="TMS320C6678_0" xml="C6678.xml" xmlpath="devices"/>
</platform>
</connection>
</configuration>
</configurations>
Trace from an attempt that stopped during Run->Connect target:
M 16:02:06:455 | cTools: cToolsMgrIF is created M 16:02:06:455 | cTools:cToolsIF.dll is delay loaded M 16:02:06:455 | cTools: main Thread ID 2904 . M 16:02:06:455 | cTools: cToolsJobMgrIF is created
Trace from an attempt that passed Run->Connect Target, but failed when tyrying to view CPU registers:
6683.ti_trace_log_7152013_3700.txt
An attempt to upgrade CCS and all components failed, during a step I got incompatible components, some sort of version problems. I did not write down the procedure I was following, nor at what stage it failed.
Help is needed!
Odd T.