This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Code Composer Application has stopped working

Hi,

I have cc v 3.3. When I attempt to start up the program, I get a message saying that "Code Composer Application has stopped working". (See attachment) The only options it gives me are to close the program. The problem details are shown as:

Problem signature:

  Problem Event Name: APPCRASH

  Application Name: cc_app.exe

  Application Version: 5.98.0.219

  Application Timestamp: 457d056a

  Fault Module Name: cc_app.exe

Fault Module Version: 5.98.0.219

  Fault Module Timestamp: 457d056a

  Exception Code: c0000005

  Exception Offset: 0020ff53

OS Version: 6.1.7601.2.1.0.256.48

  Locale ID: 1033

  Additional Information 1: 0a9e

  Additional Information 2: 0a9e372d3b4ad19135b953a78882e789

  Additional Information 3: 0a9e

  Additional Information 4: 0a9e372d3b4ad19135b953a78882e789

Read our privacy statement online:

 

http://go.microsoft.com/fwlink/?linkid=104288&clcid=0x0409

If the online privacy statement is not available, please read our privacy statement offline:

 

C:\Windows\system32\en-US\erofflps.txt

 

I'm wondering what I can do about this.

Thanks,

Brian M

  • Hi Brian,

    I see you are running on Windows 7. CCSv3.3 was never supported on Windows 7. Some people have had good success with it, others not so much. people in the latter category have resorted to running CCSv3.3 from an XP virtual machine.

    Otherwise, I'm afraid there is not much we can do here. CCSv3.3 is an unsupported product, hence it is very unlikely that any cause of crashing will not be addressed. Sorry.

    ki