This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv5 Project -> Link files to Project

[original thread at: http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/t/139999.aspx]

Rafael,

Can you please guide where the above option is available in CCS v5.4.

Thank you,

Jaspreet

  • Jaspreet,

    CCSv5.4 still has the same option as mentioned in the thread referenced - i.e., if you right-click on the project there is an option named Add Files. Selecting it will bring a browse window that will allow you to select the desired files to be added and, when clicking OK (or Open), then the referenced dialog box will be shown.

    If that does not show for you, can you try to open a different workspace and/or reset the one you are currently working (menu Window --> Reset perspective).

    BTW, if you are curious about the variable option, check the page below:

    http://processors.wiki.ti.com/index.php/Creating_portable_projects_in_CCSv5

    Hope this helps,

    Rafael

    P.S. Avoid reopening old threads, as your question will almost surely be missed.

     

  • Hi Rafael,

    Thank you for the input.

    But I found out by myself that in CCSv5.4 I can link the files by right-clicking the project -> new file -> file. In the file option if you click Advanced and by ticking Link to file in the file system , I can link files to the system easily.

    I didn't want to add the files to the project.

    Thank you for mentioning the concept of variables.

    Sincerely,

    Jaspreet