Other Parts Discussed in Thread: TM4C123GH6PM, TM4C1233H6PM
I'm moving some old projects for the Stellaris Launchpad over to my new Tiva launchpad and am having an issue. Everytime I enter the debug perspective the green resume arrow is greyed out and can't be interacted with. There are no build errors and the project is correctly migrated to TivaWare from StellarrisWare as if I make the Target device a Stellaris LM4F120H5QR and put it on the old launchpad it works fine. But once I change the target device to a Tiva TM4C1233H6PM and try to put it on the old launchpad or to a Tiva TM4C123GH6PM and put it on the new launchpad it doesn't work. Is there something that I need to do to enable the Stellaris in-circuit Debugger to work with Tiva parts? I'm running 5.4.0.00091 and have run Checked for and installed all updates from the help menu in CCS.