This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

eZdsp5505 Getting Started

Hello,

 

I am running into some issues getting started with the eZdsp5505 stick. I am running the most recent version of CCS v5.4.00091 on a Windows 7 machine, however I am having trouble building any of the examples. I am getting a build error as follows:

Description Resource Path Location Type <a href="file:/C:/ti/ccsv5/tools/compiler/dmed/HTML/10099.html">#10099-D</a>  program will not fit into available C5505.cmd /HelloWorld line 74 C/C++ Problem

Console printout:

**** Build of configuration Debug for project HelloWorld ****

"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all

'Building file: ../hello.c'

'Invoking: C5500 Compiler'

"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --include_path="C:/ti/ccsv5/tools/compiler/c5500_4.4.1/include" --define=c5505 --display_error_number --diag_warning=225 --ptrdiff_size=16 --preproc_with_compile --preproc_dependency="hello.pp"  "../hello.c"

'Finished building: ../hello.c'

' '

'Building target: HelloWorld.out'

'Invoking: C5500 Linker'

"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/bin/cl55" -v5515 --memory_model=large -g --define=c5505 --display_error_number --diag_warning=225 --ptrdiff_size=16 -z -m"HelloWorld.map" --stack_size=0x200 --heap_size=0x400 -i"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/lib" -i"C:/ti/ccsv5/tools/compiler/c5500_4.4.1/include" --reread_libs --display_error_number --warn_sections --xml_link_info="HelloWorld_linkInfo.xml" --rom_model --sys_stacksize=0x200 -o "HelloWorld.out"  "./hello.obj" -l"libc.a" "../C5505.cmd"

<Linking>

"../C5505.cmd", line 74: error #10099-D: program will not fit into available

   memory.  placement with alignment/blocking fails for section ".text" size

   0x4071 page 0.  Available memory ranges:

   DARAM1       size: 0x2000       unused: 0x2000       max hole: 0x2000   

error #10010: errors encountered during linking; "HelloWorld.out" not built

gmake: *** [HelloWorld.out] Error 1

gmake: Target `all' not remade because of errors.

>> Compilation failure

**** Build Finished ****

 

I have tried running through the getting started pages, but I ended up having to throw this one to the community. I appreciate the help.

-Jameson