when doing a certain job i am often setting up a memory window to keep certain data in a permanent watch.
when setting up the first sub-tab for the memory tab then i am selecting some base address and a data format. Enter or go-button will make it apear...
but when setting up a second item the data format is not cloned from the first one (which would be rather rational and handy) but some default format is choosen. - this could see improvement as its likely that a certain format selection will be re-used in the next window as well.
when having several such sub-tabs open i am not able to re-arrange their order at all. no dragging possible. - this could be quite helpful feature as all other tabs already do support it.
when clicking along serveral sub-tabs the headline of those tabs might be very is often abbreviated and no hint for what the full line would be. neither is there any way for editing the headline into some easy to remember name nor is the current formula that leads to the display editable. the properties tab i have open simply apears to be empty. - this could be improved. image analyzer is a good example on how it can be done. (the input box for the address formula often displays data from some other operation, but it does help only with some luck to get the prior inputs by its drop down button. in fact the input box is often misleading about whats displayed as it is not at all in sync with the current window. compare to common web browsers - the visible & editable address window is bound to the tab and changes to the new context when clicking other tabs.)