Other Parts Discussed in Thread: AM3359, AM3352, OMAP3503
Hello Forum,
I am using CCS v5.4 and Industrial SDK 1.0.0.8 to develop some applications on an AM3359 (ICE Evaluation board) with SYS/BIOS.
I created a new CCS C-Project based on the "Typical" SYS/BIOS configuration template and added some code with Single Precision Floating Point operations.
With standard settings the compiler created instructions for the VFP unit and not for the faster NEON engine. (Because of the IEE754 conformance I guess)
The following (useless) testfunction works good for demonstration:
float tstfn (float k)
{
float x = 10005.7;
float y = -22.055;
float z = 0;
z = (x + k) * y;
return z;
}
The Disassembly is:
229 {
tstfn:
80005c54: F1AD0D10 SUB.W R13, R13, #16
80005c58: ED8D0A00 FSTS S0, [R13, #0]
230 float x = 10005.7;
80005c5c: 483E LDR R0, $C$FL1
80005c5e: 9001 STR R0, [SP, #0x4]
231 float y = -22.055;
80005c60: 483E LDR R0, $C$FL2
80005c62: 9002 STR R0, [SP, #0x8]
232 float z = 0;
80005c64: 483E LDR R0, $C$FL3
80005c66: 9003 STR R0, [SP, #0xC]
233 z = (x + k) * y;
80005c68: EDDD0A00 FLDS S1, [R13, #0]
80005c6c: ED9D0A01 FLDS S0, [R13, #4]
80005c70: EE300A80 FADDS S0, S1, S0
80005c74: EDDD0A02 FLDS S1, [R13, #8]
80005c78: EE200A80 FMULS S0, S1, S0
80005c7c: ED8D0A03 FSTS S0, [R13, #12]
234 return z;
80005ee4: ED9D0A03 FLDS S0, [R13, #12]
235 }
I'm using the TI v5.0.4 compiler, downloanded with CCS with the directives:
-mv7A8 --code_state=16 --float_support=VFPv3 --abi=eabi -me -Ooff -g --define=am3359 --define=omap3503 --define=am3352 --diag_warning=225 --display_error_number --diag_wrap=off --neon
As you can see optimizations are disabled (and enabling change anything on using VFPU opcodes) and the --neon directive is added.
My question is: How must the Compiler settings be changed to get NEON instructions?
-> I am aware of the wiki page: http://processors.wiki.ti.com/index.php/Cortex-A8, which says that the "-mf" directive should also be added. But the Compiler settings do not show this option. Using the GNU compiler instead doesn't work with the SYS/BIOS libs.
-> Refering to this post http://e2e.ti.com/support/arm/sitara_arm/f/791/t/216069.aspx, I see in the Debug View of CCS that in "ARM Advanced Features" the "NEON enabled" box is set.
I hope someone can help me enabling NEON Floating Point execution on AM335x with TI-ARM Compiler in SYS/BIOS Application.
Regards, Tim