Hi
I’m using computer with WIN-7, 64 bits and I need to install on it CCS version 3.1.
I tried to install it over windows XP mode virtual PC and receive Error 1335 during installation.
The error description is: "The cabinet file 'xdas28_example_sim28xx.cab required for this installation us corrupted.
I tested this cab and it is not corrupted (I managed to open it ).
Is there a way to overcome this problem (ignore cause additional error – error 2350 and stop the installation)
Thanks
Rubi Kalev