This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS .map file format

Hi,

I have two problems as below in CCS .map format, anybody help me checked it? thanks

First:

How I do to display the length of user’s variables in .map file?  As below:

 

Customer need to format:

*********************************************************************************************

OBJECT LIST SORTED BY ADDRESS

     Name                                      Addr   hSize   dSize     Ref    Section   RLIB

---------------------------------------------------------------------------------------------

     _PORTAB                                      0       2       2      14   .abs_section_0

     _DDRAB                                       2       2       2       2   .abs_section_2

     _PORTE                                       8       1       1      11   .abs_section_8

     _DDRE                                        9       1       1       2   .abs_section_9

     _MODE                                        B       1       1       1   .abs_section_b

     _PUCR                                        C       1       1       1   .abs_section_c

     _RDRIV                                       D       1       1       1   .abs_section_d

     _GPAGE                                      10       1       1       0   .abs_section_10

     _DIRECT                                     11       1       1       0   .abs_section_11

     _MMCCTL1                                    13       1       1       0   .abs_section_13

     _PPAGE                                      15       1       1       1   .abs_section_15

     _RPAGE                                      16       1       1       0   .abs_section_16

     _EPAGE                                      17       1       1       0   .abs_section_17

     _PARTID                                     1A       2       2       0   .abs_section_1a

 

Our CCS format have not each variable length information:

*********************************************************************************************

GLOBAL SYMBOLS: SORTED BY Symbol Address

address    name

--------   ----

00000000   _ti_ascii

00000001   __TI_args_main

00000050   __stack

00000200   __SYSMEM_SIZE

00000300   __STACK_SIZE

00000350   __STACK_END

00000400   __sys_memory

00000600   __CIOBUF_

00000e3d   __ctypes_

00000f3e   _PIE_tableDebugInit

000010a0   _pucTempString

000010b5   _escRed

 

Reasons:

This information is used for communication between PC and product when customer is debugging the parameters of product,  the debugging work will be very bother if don’t have this information. Because customer will copy .map content to PC to change the value of the current parameter is sent directly to its address without complex protocols.

 

Second:

How to set up to make the .C file continuous variables defined in flash is stored contiguously? Example:

 

I was defined the variables as below:

 

 

Source:

/*****************************************************************************/

① Uint16  cnt;

② Uint16  Status;

③ Uint16  *Flash_ptr;     // Pointer to a location in flash

④ Uint32  Length;         // Number of 16-bit values to be programmed

⑤ float32 Version;        // Version of the API in floating point

⑥ Uint32  Flash_32Bitdata[5];     // Version of the API in decimal encoded hex

⑦ Uint32  *Flash_32Bitdata_ptr;     // Pointer to a location in flash

/*---------------------------------------------------------------------------

  Sector address info

---------------------------------------------------------------------------*/

typedef struct {

     Uint16 *StartAddr;

     Uint16 *EndAddr;

} SECTOR;

 

⑨SECTOR Sector[4] = {

         (Uint16 *)0x3F7000,(Uint16 *)0x3F7FFF,

         (Uint16 *)0x3F6000,(Uint16 *)0x3F6FFF,

         (Uint16 *)0x3F5000,(Uint16 *)0x3F5FFF,

         (Uint16 *)0x3F4000,(Uint16 *)0x3F4FFF,

};

// -------------------------------- FRAMEWORK --------------------------------------

// State Machine function prototypes

//----------------------------------------------------------------------------------

//

//

// ---------------------------------- USER -----------------------------------------

// ----------------------------                    ---------------------------------

//system initial use

 

unsigned long Duty_Range = 0;

unsigned long Duty_Value = 0;

unsigned int  Duty_H = 0;

unsigned int  Duty_L = 0;

unsigned long Timer2_value;

/*****************************************************************************/

 

Currently .map  address about them as below

/*****************************************************************************/

⑬  00008bc0   _Duty_L

① 00008bc1   _cnt

② 00008bc2   _Status

⑫ 00008bc3   _Duty_H

   00008bc4   _testA

⑭ 00008bc6   _Timer2_value

   00008bc8   _MEP_ScaleFactor

③ 00008bca   _Flash_ptr

⑤ 00008bcc   _Version

   00008bce   _Duty_Range

   00008bd0   _Flash_32Bitdata_ptr

⑪ 00008bd2   _Duty_Value

④ 00008bd4   _Length

   00008bd6   _FlashStatus

   00008bda   _ePWM

⑦  00008bde   _Flash_32Bitdata

⑨ 00008be8   _Sector

   00008bf8   __cleanup_ptr

   00008bfa   __dtors_ptr

   00008bfc   _PieVectTableInit

   003d7fff   _PartIdRegs

   003f7ff8   _CsmPwl

   003ff8d2   _Flash2802x_Program

   003ff98e   _Flash2802x_Erase

/*****************************************************************************/

 

Customer needed as below:

/*****************************************************************************/

① 00008bc1   _cnt

② 00008bc2   _Status

③ 00008bca   _Flash_ptr

④ 00008bd4   _Length

⑤ 00008bcc   _Version

Etc..

/*****************************************************************************/

 

Thanks…..