Hi,
I find that CSL 3.03 for eZDSP5535 on a CCS v5.4 cannot compile on a Windows 7, 64 bit PC.
Then, I install CCS v4.2 and CSL3.01 on a XP PC, it doesn't work either. (Today I find that there is no the target for ezdsp 5535 with CCS v4.2)
I install CCS v.5.2 on this XP yesterday. It does have ezdsp5535 target, but I find that it cannot finish connection test. It stops after showing:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity
[Result]
-----[Print the board config pathname(s)]------------------------------------
C:\DOCUME~1\Jeff\LOCALS~1\APPLIC~1\.TI\213602635\
0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 100- or 510-class product.
This utility will load the adapter 'jioserdesusb.dll'.
The library build date was 'Mar 18 2012'.
The library build time was '21:43:48'.
The library package version is '5.0.663.0'.
The library component version is '35.34.39.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
Comparing with that of Windows 7, I find that there is no "~" on win7 path display.
What is the problem? Thanks