I have a customer with the following question about an older OMAP processor and how they can get a version of CCS to run on Windows 8, can someone help? Thank you!
We have recently upgraded our computers and have run into an unexpected issue. It seems that the OMAP we are using (a variant of the 2430) is NOT supported by any version of Code Composer newer than 3.3. But CCS3.3 is very difficult, if not impossible, to get running on Windows8, which is the only OS now available on modern computers. So this leaves us in a rather difficult and precarious situation, being unable to develop software for our hardware platform. What do you suggest? Thanks!