This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS install error on Windows 7 based PC

CCS install error on Windows 7 based PC

Following picture shows an error message window.

What should I do to install without this message window?

  • Hi,

    32 or 64bit?

    Regards,

    Gautam

  • Hi Ahnsei,

    are you trying with the current release, v5.4?  Would it be possible for you to

    1 - please send us the install logs.  these are in the installjammer registry directory.  the folder may be hidden and is under program files or program files(x86).

    2 - try again with the full v5.4 installer and antivirus disabled to a fresh directory with no special characters

    Best Regards,
    Lisa 

  • Following attach shows my system info_

     

    Thanks.

  • Attached picture show you the version of IDE.

     

    1 - Would you let me know more specific way to get the install logs?

  • Hi,

    once again ... please try with the latest version.  Log instructions are also here for you:

    1 - please send us the install logs.  these are in the installjammer registry directory.  the folder may be hidden and is under program files or program files(x86).

    2 - try again with the full v5.4 installer and antivirus disabled to a fresh directory with no special characters

    Best Regards,
    Lisa 

  • I just want to use our own purchased CD.

    Printed words on the purchased CD shows Windows, XP, VISTA, 7

    Is there any specific reason for using the latest version not my version?

     

    Thanks.

  • Hi Ahnsei,

    there are two reasons to use the newest version

    1 - latest bug fixes and support.  support is more limited for older versions

    2 - there is a known issue installing from cds anyhow

    Best Regards,
    Lisa 

  • Thanks for your advice.

    1. I cannot get another version.

    2. As you(TI) wrote the word(Window7) on CD that I purchased, I think you shold guarantee the operation of the CCS on window 7 based PC with my CD.

    Put yourself in my shoes, even I purchased the CD insisting it can run on window7, why should I have to put more effort?

    You give me advice whenever I raise an issue, but the advice is hard to me to do and it is abstract.

    I think, you need to give advice with more details.

     

    Best Regards,

    Ahnsei.

     

     

  • Hi Ahnsei,

    yes, unfortunately the cds are thought to be a service, however as you see there are numerous issues.  By the time of shipment they are out of date and the issues I mentioned we found with the installer.

    I would do the following

     1 - clear out any old installations.  Do this manually by deleting the ccsv5 directory (or ccsv4).  Also delete the logs from the installjammer registry directory.  This is a potentially hidden folder in program files or program files (x86).

    2 - download the latest version from this site.  Not the large button but a bit further down to ensure you have the offline installer

    http://processors.wiki.ti.com/index.php/Download_CCS

    3 - fully unzip and install v5.4 to a fresh simple directory with antivirus disabled.

    If you have any issues send us the logs from the installjammer registry directory mentioned in step 1.

    Best Regards,
    Lisa