I recently purchased a licesce for CCSVersion: 4.0.2.01003 after familiarizing myself with the demo version of CCS V3.3. With the new version, I'm having more problems than I can possibly begin to list here, but one error I get is:
fatal error: file "../qmath.lib<qsqrt.obj>" specifies ISA revision "C2700", which is not compatible with ISA revision "C2800" specified in a previous file or on the command line
I am using a 320TMSF2812, and the qmath library that I am using worked with CCS 3.3, and is designed for the C28XX processor. Why doesn't it work in CCS4.02?
P.S. Is there any way I can trade in my licence for CCS4.0 with a license for CCS3.3? This would be by far the quckest way for me to get going again.