Hi there.
Is there another way to force CCS to run in background than to go to Window->Preferences->General and select "Always run in background" if I don't want to set this everytime I restart CCS and start building?
BR, Carsten
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi there.
Is there another way to force CCS to run in background than to go to Window->Preferences->General and select "Always run in background" if I don't want to set this everytime I restart CCS and start building?
BR, Carsten
Hi Carsten,
You only need to set it once per workspace, every restart of CCS will have this setting saved in your workspace preference.
Also, when there is a progress dialog pops up, there is a checkbox option within the progress dialog. Checking this option will put the dialog and future dialog in the background.
Are you looking for a way to have this option set to enable or disable by default for new workspace?
Regards,
Patrick
Sorry.. send too fast. What version of CCS are you using? I was able to have this option persisted after I shutdown CCS and restart?
Regards,
Patrick
Hi Patrick.
I'm running CCS Version: 5.4.0.00091.
It might be caused due to the fact that we're running GIT on our project. Can you tell me where the workspace prefs are saved?
BR, Carsten
Hi Carsten,
The workspace preferences are stored in the workspace under ".metadata\.plugins\org.eclipse.core.runtime\.settings\org.eclipse.ui.workbench.prefs" file.
There is a bug filed against this issue already, SDSCM00047846.
If you want to default this setting for every new workspace, you can try adding the following line to the ccsv5\eclipse\plugins\com.ti.ccstudio.branding_xyz\plugin_customization.ini file. I haven't try it myself, so I am not sure if this workaround will work or not.
org.eclipse.ui.workbench/RUN_IN_BACKGROUND=true
Regards,
Patrick