Other Parts Discussed in Thread: MSP430F5152
Good day,
I have been using CCS V5.4 for developing using the MSP430 devices, no problems here, however I would now like start using the C2000 (Piccolo series).
For the MSP430 work I am making use of the "Code Limited" license version, which won't allow me to use the C2000 series.
Also if i install CCS V5.4 for the C2000 series then the MSP430 series is not available.
Must I install 2 versions of CCS V5.4, one for each series (in a different location)?
Will this work?
Or what is the best solution, without having to purchase a license?
I haven't tried the the dual installation because I am busy with critical development using the MSP430 series, and can't afford to lose this working setup.
Thank you in advance.
Mike