This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6678 Error connecting to Target with Blackhawk XDS560v2

Howdy, thanks in advance for any help.

I am having an issue setting up my Blackhawk XDS560v2 System Trace debugger with my C6678 DSPs on the Advantech DSPC-8681E.  The following error appears when I attempt to debug in CCS:

IcePick_D: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/r try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.1.73.0)

My CCS version is:  5.4.0.00091.

So far, I have reset the device (via the Blackhawk BH560v2 Config Utility software) and I have lowered the TCLK in CCS from default 10.368MHz to 100kHz.

I have also created a new .ccxml file, hoping that might help.

When I run the "Test Connection" in the .ccxml "Advanced" page, I do not get any errors.

Where should I start to try and understand why it can't access the device register?