Other Parts Discussed in Thread: CCSTUDIO
Hi Friends,
i have long persisting error , i have this error when ever i try to rebuild the example application. i don't know what was i done wrongly.
I'm using CCSv3.3 and dvsdk_1_00_00_19\examples. can anyone suggest me idea to solve this issue? Im looking forward...
[_gen.c] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -@"=C:/dvsdk_1_00_00_19/examples/video_encdec_fio_jnvi/config/_gen.opt" -pdr -o3 -fr"C:/dvsdk_1_00_00_19/examples/video_encdec_fio_jnvi/Debug" -i"C:/dvsdk_1_00_00_19/examples/video_encdec_fio_jnvi" -i"." -i"C:/dvsdk_1_00_00_19/xdctools_2_91_00_01/packages" -i"C:/dvsdk_1_00_00_19/codec_engine_1_20/packages" -i"C:/dvsdk_1_00_00_19/xdais_5_20/packages" -i"C:/CCStudio_v3.3/boards/evmdm6437_v2/include" -d"_DEBUG" -mv6400+ -@"../Debug.lkf" "_gen.c"
Fatal error: could not open source file "_gen.c"
1 fatal error detected in the compilation of "_gen.c".
Compilation terminated.
>> Compilation failure
[_gen_bios.s62] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -g -@"=C:/dvsdk_1_00_00_19/examples/video_encdec_fio_jnvi/config/_gen.opt" -pdr -o3 -fr"C:/dvsdk_1_00_00_19/examples/video_encdec_fio_jnvi/Debug" -i"C:/dvsdk_1_00_00_19/examples/video_encdec_fio_jnvi" -i"." -i"C:/dvsdk_1_00_00_19/xdctools_2_91_00_01/packages" -i"C:/dvsdk_1_00_00_19/codec_engine_1_20/packages" -i"C:/dvsdk_1_00_00_19/xdais_5_20/packages" -i"C:/CCStudio_v3.3/boards/evmdm6437_v2/include" -d"_DEBUG" -mv6400+ -@"../Debug.lkf" "_gen_bios.s62"
"_gen_bios.s62", ERROR! : [E1000] Cannot open source file _gen_bios.s62: No
such file or directory
>> Compilation failure
Build Complete,
2 Errors, 0 Warnings, 0 Remarks.
thnx
VS