This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how to remove corrupt CCS

I installed CCS and had a problem so I tried to uninstall it with "Programs and Features" (I'm on Windows 7 x64).  The uninstall went about half way and stopped.  After several hours I gave up and tried to cancel it.  The system was totally unresponsive event to the mouse.  I had no option other than to do a hard shut down.  Now CCS is in a partially installed state.  I doesn't show up in "Programs and Features" or in the start menu, but when I try to install CCS, the install tells me that it is already installed and to uninstall first.

Now I need to manually remove files and folders and to clean up the registry.  Can anyone tell me what I need to delete?  I really don't want to reformat my hard drive.