Other Parts Discussed in Thread: UNIFLASH
Hi everyone....
I'm getting some problems to install the "Uniflash Standalone Flash Tool"...
Could someone help me?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Marcio,
is this as part of a general ccs installation do you mean? Would you be able to send us the installation logs? These are found in the installjammer registry directory which may be hidden and is under program files or program files(x86).
Best Regards,
Lisa
Hi Lisa,
I was trying to install the "Uniflash Standalone Flash Tool" for CCS V3. So this error appears...
I couldn't find the installation logs...
I tried to download and install the Microsoft Visual C++ 2008 but it still didn't work
Hi Marcio,
Could you install the redistributable package separately from the C:/Documents and Settings/marcio/Desktop/UNIFLASH2.2.0.00016_win32/baserepo/ folder first. Then do a clean install. You may want to move the repo C:/Documents and Settings/marcio/Desktop/UNIFLASH2.2.0.00016_win32 to a folder without spaces too, though I don’t think that will be a problem, it’s safer.
Please keep us informed how that goes.
Best Regards,
Lisa
Hi Lisa,
I succeed to install the program...
but I've another problem...
after configuring I have been trying to load the program and I got this errors:
[15:54:01] Begin Writing flash memory operation...
[15:54:01] Loading program: C:\Documents and Settings\marcio\Desktop\Teste49201vs100\Teste49201vs100.out
[15:54:09] ERROR >> C28xx: Error: Error 0x20001020/-1135 Severe Error during: Execution, Target, Unrecoverable emulation error
[15:54:21] ERROR >> C28xx: Can't Run Target CPU: Error 0x00000020/-1140 Error during: Execution, JTAG protocol reset, detected TRSTn assertion.
[15:54:21] ERROR >> C28xx: File Loader: Data verification failed at address 0x003F7FF6 Please verify target memory and memory map.
[15:54:21] ERROR >> C28xx: GEL: File: C:\Documents and Settings\marcio\Desktop\Teste49201vs100\Teste49201vs100.out: a data verification error occurred, file load failed.
[15:54:21] File: C:\Documents and Settings\marcio\Desktop\Teste49201vs100\Teste49201vs100.out: a data verification error occurred, file load failed.
[15:54:22] Operation Writing flash memory returned.
It's look like the error I usualy have using the CCS V3 and "Tools/F28xx On-Chip Flash Programmer".
But there I got the first error... so I do a "Cancel option"...
and do a .gel comand "GEL/Reset"...
at this point the disassembly window points to "3FF8A1 28AD004 MOV @SP,#0x0004" so I succeed to program.
Could you tell me if I'm doing something wrong?
Thanks for the attention.
HI Marcio,
it seems you may have an odd initialization problem. Unfortunately you can't call a gel command from uniflash.
Could you try the following: try the same procedure that worked in v3 but using ccs v5.4 instead of uniflash. Please keep us informed how that goes.
Best Regards,
Lisa
Hi Lisa,
unfortunatly I wouldn't... I'm in another project development that is stoped for a time and I'm afraid to install the CCS V5... because I think it can bring me some problem when I back to the project.
I was just trying a faster way to program the a DSP...
Do you have some TI programmer for DSP?
Thank you!
Hi Marcio,
there are really not any other TI options, but there is an option from spectrum digital you might be able to try.
http://emulators.spectrumdigital.com/utilities/sdflash/
Best Regards,
Lisa