This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C callable function in asm can have both function with _ and without _?

Hi,

The code below dot line is from Page 82/332, spru186v.pdf. It can be run and debug days ago. Then, my computer shutdown by itself. After reboot and hard disk recovery, this project cannot run again. Now, it can only run without _ with eabi option.

I create a separate project with COFF option. It can run without _ for both userfunc and printf functions. So, for mixed with userfunc and _printf, what option can make it runnable?

Thanks,

 

 

........................

1 00000000 .sect ".text"

2 .global userfunc

3 .global _printf

4

5 userfunc: .asmfunc stack_usage(16)

6 00000000 00000010! CALL .S1 _printf

7 00000004 01BC94F6 STW .D2T2 B3,*B15--(16)

8 00000008 01800E2A' MVKL .S2 RL0,B3

9 0000000c 01800028+ MVKL .S1 SL1+0,A3

10 00000010 01800068+ MVKH .S1 SL1+0,A3

11

12 00000014 01BC22F5 STW .D2T1 A3,*+B15(4)

13 00000018 0180006A' || MVKH .S2 RL0,B3

14

15 0000001c 01BC92E6 RL0: LDW .D2T2 *++B15(16),B3

16 00000020 020008C0 ZERO .D1 A4

17 00000024 00004000 NOP 3

18 00000028 000C0362 RET .S2 B3

19 0000002c 00008000 NOP 5

20 .endasmfunc

21

22 00000000 .sect ".const"

23 00000000 00000048 SL1: .string "Hello World!",10,0