Hi,
The XDS100v2 JTAG emulator (and the on-board emulator of the ICE dev kit) are based on the FTDI FT2232 chip.
However, FTDI has a newer FT4232H chip (having more channels). Is that possible to use it as onboard emulator?
1. Except for VID/PID configuration, is there any TI specific firmware/CPLD image downloaded into the FT2232 chip or only FTDI supplied (by default) code is used?
2. There are some pins connected to FTDI GPIO (EMU0/1, SysReset), what defines the mapping of these on PC side? Can this mapping be altered?
Best,
Vasili