Other Parts Discussed in Thread: TMS320C6670
Hi all,
i want to make emulation on TMS320C6670 using built in emulator XDS100 v1 ,
i have also CCS v5.3 , i configured the target configuration file to support my device,
but i am faced error
IcePick_D: Error connecting to the target: Cannot access register at 0x00000000 (Error -2131) @ 0 (0x0)
Then to be sure that PC see the connection , i am going to the device manager i found it configured correctly .
Using Debug Jtag IDE to be sure how to debug whether the JTAG scan path is broken , i faced the error
----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver.
The value is '-183' (0xffffff49).
The title is 'SC_ERR_CTL_CBL_BREAK_FAR'.
The explanation is:
The controller has detected a cable break far-from itself.
The user must connect the cable/pod to the target.
Any help please,
Thanks in advanced .
Muhammed .