Team,
I have a customer who has filed the following support request. Can you provide any help?
I try run Loggerstreamer module as part of my application running on c6678 target.
The code is based on TI tutorial as described in
http://processors.wiki.ti.com/index.php/System_Analyzer_Tutorial_5A. My cfg file
configuration is the same as in the tutorial and my related prime and exchange c code
functions are also the same. My application calls Log_printUC/Log_info APIs.
When running on the my target I can see that the buffers are being populated and the
exchange function works. I have also been able to pull out the buffers from the target via
XDS debugger using the script provided in the tutorial.
However when trying to open the bin file created using the system analyzer in CCS5.2
there are no logs displayed. The UIA Config File used is either from the auto detection
mechanism in CCS or the one I created.