Other Parts Discussed in Thread: SYSBIOS
Hi,
Using the menu command RTSC Tools - Platform - Edit/View, I edited an existing platform( I changed DDR into IRAM in the Memory Sections of ti.platforms.evm6748.) and pressed the Finish button, which gave a message that "Platform package 'ti.platforms.evm6748' built successfully in repository....".
After that, while rebuilding the project, the following error message occurred.
"js: "C:/ti/xdctools_3_25_00_48/packages/xdc/cfg/Main.xs", line 153: Error: incompatible use of package 'ti.platforms.evm6748' [in C:/ti/xdctools_3_25_00_48/packages/ti/platforms/evm6748/]: version of the loaded package 'ti.platforms.evm6748' is [], while 'ti.sysbios' [in C:/ti/bios_6_33_05_46/packages/ti/sysbios/] was built with 'ti.platforms.evm6748' [1, 0, 0, 1335304647185]"
Xdctools_3_25_00_48 and bios_6_33_05_46 have been installed and selected in CCS. What went wrong?
Shoudn't existing platforms be edited or changed? By the way, there was no problem in creating new platforms and using the created platforms.
My CCS version is v.5.4.0.