Hi,
I am troubling to use XDS200 Emulator with CCS5.4.
I could not connect to XDS200 Emulator to the target.
When I executed the Test Connection, I had the below result.
--------------------------------------------------------
Result]
-----[Print the board config pathname(s)]------------------------------------
C:\DOCUME~1\KTL329\LOCALS~1\APPLIC~1\.TI\
693494126\0\0\BrdDat\testBoard.dat
-----[Print the reset-command software log-file]-----------------------------
This utility has selected a 560/2xx-class product.
This utility will load the program 'xds2xxu.out'.
E_RPCENV_IO_ERROR(-6) No connection: DTC_IO_Open::dtc_io
Failed to open i/o connection (xds2xxu:0)
An error occurred while soft opening the controller.
-----[An error has occurred and this utility has aborted]--------------------
This error is generated by TI's USCIF driver or utilities.
The value is '-250' (0xffffff06).
The title is 'SC_ERR_ECOM_EMUNAME'.
The explanation is:
An attempt to access the named emulator via USCIF ECOM has failed.
[End]
-----------------------------------------
Also I checked the device manager. Please see the below.
So I think the driver installation is no problem.
And then, I had failure message as the below when I tried to connect to the target.
I don't know what is the wrong.
Please advise me.
Best regards,
Michi