This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question Regarding C55x assembler

Hello

Iam Extremely new to assembly programming of code composer in event of using rtc interrupt i have some code in which the project is in large memory model and i am getting pretty intersting problems with the code taken from a demo project for the interrupt vecotrs

here i have attached the interrput vector assembly file  7612.rtc.asm which is throwing me problems  

here below are the errors i am not able to resolve them 

"../Delay-Testing/rtc.asm", REMARK at line 187: [R5672] If there is a long MMR
write with no
intervening single
MMR before this
return from
interrupt, then an
interrupted
conditional execution
may be corrupted;
(see the C55x silicon
exceptions errata;
Advisory CPU_94)
return_int

"../Delay-Testing/rtc.asm", REMARK at line 187: [R5674] If processor is in
fast-return mode, and
this return from
interrupt instruction
is stalled in the
ADDRESS or ACCESS1
phase, then the
execution of a
subsequent
conditional execution
may be corrupted;
(see the C55x silicon
exceptions errata;
Advisory CPU_99)
return_int

"../Delay-Testing/rtc.asm", REMARK at line 187: [R5675] An MMR write to the
RPTC register that is
close to this return
from interrupt
instruction may cause
an interrupted single
repeat loop's
execution to be
corrupted; (see the
C55x silicon
exceptions errata;
Advisory CPU_100)
return_int

COOL  i hav overcomed this by reading Advisory CPU_100 and in assembly file edited this code 

@RPTC_L=pop()||mmap()
nop
nop
nop
nop
nop
nop

before retrun_int

this solved the problem