Other Parts Discussed in Thread: CCSTUDIO
I inherited an unloved, never used 'C6201 EVM and bundled software (CCStudio V1.0 released 1999) when the company closed my office.
It's now sitting quite happlly in an old Dell Dimension XPS B1000r (Pentium III 1.0GHz, 128M of RAM, 20G HDD and a fresh install of Win 98SE). The installation appeared to run without any trouble apart from having to reseat the board once and the Confidence Test passes without a hiccup. However, when running through the Tutorial I cannot locate the required library, rts6201.lib. In short the cgtools folder is missing, clearly I've missed a step somewhere or something went wrong silently.
Can anyone shed some light on this problem?
NB. I'm only wanting to use the EVM board as a platform for self-training in DSP while looking for the next job so don't want to spend money on the latest and greatest CCStudio (yet :-)).
Robert