This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Cannot edit code in ccs 5.4

I installed ccs 5.4 and made a new project. When it gets done and goes to the ide, the edit box where you put code in is greyed out. I have tried closing the program and reopening and still cannot type because it is still greyed out. I have pushed every button in the program and cant seem to get it to open where i can edit code. I checked lisence status and it says lisenced, so thats not the problem. If I open an example code, the editor works fine. But if I start a new project or open an existing project, I cant do anything.