Other Parts Discussed in Thread: SIMPLICITI, CC1101
Hi,
I have a problem (maybe it is not a problem) with .dat files in SimpliciTI RF stack. These .dat files are used for build configuration of this stack. For example:
# Define Frequency Agility as active for this build
--define=FREQUENCY_AGILITY
# Enable application autoacknowledge support. Requires extended API as well
--define=APP_AUTO_ACK
It means that FREQUENCY_AGILITY and APP_AUTO_ACK are defined. It is ok and I understand.
BUT. I show you a piece of application program for better understanding:
As you can see... in application program it seems that FREQUENCY_AGILITY is not defined because #ifdef - #endif directive is highlighted. But FREQUENCY_AGILITY is really defined - it must be, because if I insert "#" before --define=FREQUENCY_AGILITY in .dat file I get an error after build.
Is my problem with this linker or compilator setting issue? I tried to find any information in project settings, but without succes. Thank you very much.
Maros.