This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Upgrading CCSv5.4 to CCSv5.5

Hello,

At the moment I have licensed CCSv5.4 and was trying to update to CCSv5.5 using Help->Check for updates, but it is reported "No updates found", although previously upgrades worked correctly and Window->Preferences->Install/Upgrade->Available Sites has a few addresses enabled. My subscription was expired but it was upgraded recently and someone mentioned in a previous post that CCSv5.4 cannot be upgraded to CCSv5.5 without an subscription. I registered the subscription for CCS on this account and it is active until 2014. Are the updates available or I need to re-install from scratch CCSv5.5?

Best regards,

David.