This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Has anyone managed to get this installed? I know they're both a bit new, but thought I'd ask.
I've tried the web and offline installer (which bizarrely refuses to work without an internet connection). I ensured the installer ran as administrator, cleared install logs, etc. The first problem it comes across in installing the VC++ 2008 redistributable, but there are others if you get past this.
Just checked and I get the same with CCS 5.4 so it's probably a general Windows 8.1 compatibility thing.
Hi Fred,
could you please send the installation logs? These are in the installjammer registry directory. The folder might be hidden and is under program files or program files(x86).
Best Regards,
Lisa
Log attached.
I managed to get it installed by doing the following. Not sure which part did the trick!
Hope that helps anyone else doing the same.
Fred
Hi Fred,
great to hear and thanks for the update. I suspect it was either the UAC or flaky connection betwee C and D last time.
All the best with development..
Best regards,
Lisa