Hi,
I'm trying to connect CCS V3.3 with my DM6437 board on Windows 7, but every time I try to connect it, the following error pops up.
I/O Port = 540
Board Name: EVM DM6437
Cpu Name: CPU_1
Abort: Close Code Composer Studio.
Retry: Try to initialize the emulator again.
Ignore: Ignore the initialization error and start
potentially without target debugging access.
Diagnostic: Run diagnostic utility.
when I ignore it, it just won't connect to the Board.
when I click on Diagnostic following dialog box appears:
Diagnostic Utility: "" failed to load
what should I do now?