Is the EVM board mandatory or not?
I haven't EVM board, could i just test OpenMP via software simulator? do you have such kind of simulator? If yes, where is the guide/manual?
BR&Thanks
XiangHao
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is the EVM board mandatory or not?
I haven't EVM board, could i just test OpenMP via software simulator? do you have such kind of simulator? If yes, where is the guide/manual?
BR&Thanks
XiangHao
Hi,
Here are the steps to work on OpenMP:
http://processors.wiki.ti.com/index.php/OpenMP_on_C6000
Regards,
Gautam
Thank you very much!
Yes, I read this document and it said:
This section was developed with CCS version 5.2.0.00069, MCSDK version 2.1.0.3, and executed on an C6678 EVM. If your environment differs, you may have to make a few adjustments.
Does this mean the hardware Evm board is mandatory? I haven' t Evm on hand, then I can not run this OpenMP project, is it right? Do you have software simulator to support this project or not?
BR&Thanks
Xiang Hao
Xiang Hao,
I was able to follow the procedure in the page Gautam sent and successfully run the OpenMP example in the C6678 simulator.
However, I am using CCSv5.5.0.00077 and MCSDK 2.01.02.06 and the C6678 Device Functional Simulator, Little Endian.
I also launched the simulator manually by going to menu View --> Target Configurations --> right-click on the target configuration and select Launch Selected Configuration. Then I selected the four cores (using Ctrl-left mouse click) and grouped them (with all four cores selected, right-click and select Group cores), so I could load and run the code easier.
Hope this helps,
Rafael