Other Parts Discussed in Thread: CC2538
Hi all,
While compiling the source code ,I am getting warning saying as #177-D: subscript out of range.
The below line is the one I am trying to compile,
uip_ip6addr(&unicast_conn->ripaddr, 0xfe80, 0, 0, 0, 0, 0, 0, 0);
and its macro expansion is
/**
* Construct an IPv6 address from eight 16-bit words.
*
* This function constructs an IPv6 address.
*
* \hideinitializer
*/
#define uip_ip6addr(addr, addr0,addr1,addr2,addr3,addr4,addr5,addr6,addr7) do { \
(addr)->u16[0] = UIP_HTONS(addr0); \
(addr)->u16[1] = UIP_HTONS(addr1); \
(addr)->u16[2] = UIP_HTONS(addr2); \
(addr)->u16[3] = UIP_HTONS(addr3); \
(addr)->u16[4] = UIP_HTONS(addr4); \
(addr)->u16[5] = UIP_HTONS(addr5); \
(addr)->u16[6] = UIP_HTONS(addr6); \
(addr)->u16[7] = UIP_HTONS(addr7); \
} while(0)
and It is expanding in the preprocessor as
do { (&unicast_conn->ripaddr)->u16[0] = (uint16_t)((((uint16_t) (0xfe80)) << 8) | (((uint16_t) (0xfe80)) >> 8)); (&unicast_conn->ripaddr)->u16[1] = (uint16_t)((((uint16_t) (0)) << 8) | (((uint16_t) (0)) >> 8)); (&unicast_conn->ripaddr)->u16[2] = (uint16_t)((((uint16_t) (0)) << 8) | (((uint16_t) (0)) >> 8)); (&unicast_conn->ripaddr)->u16[3] = (uint16_t)((((uint16_t) (0)) << 8) | (((uint16_t) (0)) >> 8)); (&unicast_conn->ripaddr)->u16[4] = (uint16_t)((((uint16_t) (0)) << 8) | (((uint16_t) (0)) >> 8)); (&unicast_conn->ripaddr)->u16[5] = (uint16_t)((((uint16_t) (0)) << 8) | (((uint16_t) (0)) >> 8)); (&unicast_conn->ripaddr)->u16[6] = (uint16_t)((((uint16_t) (0)) << 8) | (((uint16_t) (0)) >> 8)); (&unicast_conn->ripaddr)->u16[7] = (uint16_t)((((uint16_t) (0)) << 8) | (((uint16_t) (0)) >> 8)); } while(0);
Please let me know how to get rid that warning.
Thanks ,
Jagas