We have a customer that has developed a system based on the the L138 and C6748. They also developed a test application. Their application as it stands now is based on the following tools & software and Code Composer Studio 4 (these versions are what is checked into their version control system)
SW Version
SYS/BIOS 6.32.03.43
C6000 compiler 7.3.0
UIA 1.01.00.04
XDC Tools 3.22.02.27
TMS470 Not sure
IPC ??
They have an opportunity now to update to the latest and greatest with the least amount of risk to their program and may not see this opportunity again as it’s usually not “scheduled” as part of the development effort. They have the following questions:
- It looks like versions are updated often (at least the compiler), is there a set frequency/schedule TI has for the various tools releases, if so what is that?
- Will they have problems getting support from TI if they are on an older version like the 1st set of tools above (see attachment) which are the oldest?
- What risk is there in going from the 1st set to the 3rd set (see attachment for the 3 sets)?
- Are there any dependencies? Like if they want to mix and match various versions, are there any specific dependencies we need to be aware of or combinations that don’t work?
- Is the 7.3 compiler more stable than the 7.4 version? Why would they choose one over the other?
I realize that this forum is just for TI C/C++ Compiler and that you may not be able to respond to all of the tools listed above.
Thanks for your help.
Regards,
John Wiemeyer