I just got TMDSEVM6657LS. I have installed CCS5.5.0.00077_win32. My OS is win 7 64-bit.
This is the first time for me to deal with dsp, but i am experienced with microcontroller and ARM processor (even though it is not TI product).
When I tried to debug "hello word" example, there was an error:
"IcePick_D: Error initializing emulator: (Error -2083 @ 0x0) Unable to communicate with the emulator. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.1.232.0)"
And I connected the usb cable to XDS200, not the main board.
I am sure that the xds-200 driver is installed in my computer.
(I checked in Device Manager, there are 2 items : XDS2xx emulator and XDS2xx user).
What's wrong?