Other Parts Discussed in Thread: MSP430F5509, CC430F6137
Hi Lisa,
Great thanks for update. Ez430_chronos_datalogger works fine but I get an error when trying to run debug on C1_Example:
identifier "UPCS0" is undefined
Does this have to do with the fact that I am running the build configuration "915MHz - Unrestricted CCS Platinum (USA)". I couldn't find "Limited CCS Core Edition (USA)" option for it which I am currently using for Ez430_chronos_datalogger. This is the message I get after:
Error connecting to the target:
The target setup (MSP430f5509) does not match the actual target type (CC430F6137).
Best,
Sugaal