This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Delfino C++ class allocation location

I am adding an external  SRAM chip to my Delfino design (ZONE7 using XINTF).  The external SRAM is slower than internal SARAM.

I would like to place data and code in the external RAM when speed is not essential/

My Code is C++.  I can write my own malloc to allocate memory from ZONE7 (just a memory counter).

How can I do a "new" class  command to get memory from ZONE7 rather from the heap in general.  probably one of those #pragma DATA_SECTION commands.

Or do a (malloc) with the size of the class I am creating.

Is there a TI trick for this?