I have a node locked seat of CCS. 5.4 worked fine. I just upgraded to 5.5, and get "UNLICENSED" in the lower left of the eclipse window. I check licensing technical information, and it says my hostid doesn't match. Now... this is the same machine I've had for some time, so I know that's bogus. I do, however, have two NICs, so I thought it might be looking at the other NIC. I rehosted the license to that MAC address, but no joy. Still doesn't work.
My license is a permanent, uncounted license. The machine has the correct MAC address listed in the "Show Technical Information" error message. Yet for some reason, license checkout is failing.
I'm running Ubuntu 13.04, 64-bit. What gives TI?
jaredj(2009)@fourier:common $ ifconfig
eth1 Link encap:Ethernet HWaddr 00:21:9b:ff:a8:42
inet addr:192.168.120.255 Bcast:192.168.127.255 Mask:255.255.248.0
inet6 addr: fe80::221:9bff:feff:a842/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:7592987 errors:0 dropped:1213 overruns:0 frame:0
TX packets:4646113 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:3649698351 (3.6 GB) TX bytes:1207464985 (1.2 GB)
Interrupt:18 Memory:fb700000-fb720000