This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Handling IQ numbers in GUI Composer widgets



Hi, is there any built-in support for IQ numbers in widgets? AFAIK, the IQ fraction size is available in .out file, so it should be possible to automatically extract this information.

Also, when trying to display the numbers directly in a widget, I have to set the maximum value quite high. However, this makes the labels and markers on the graph very dense, so white bars are shown instead. Is it possible to specify the density or number of markers and labels?