Error in action ExecuteAction: Error in action InstallSelectedFiles: couldn't execute "/tmp/ijtmp_46FB1DF1-FBD2-1937-F732-94959FF1F5B7/installkit.bin": permission denied while executing
I am using Linux as host (Archlinux if matters), and this is a 64 bit machine with a corresponding kernel. So, my question is how to fix the aforementioned issue? I even tried to run the installer as root... but did not help.
The file I am trying to run is "ti_cgt_c6000_7.4.5_setup_linux_x86.bin"
ls -l ./ti_cgt_c6000_7.4.5_setup_linux_x86.bin
-rwxr-xr-x 1 lpapp lpapp 90271620 Oct 9 16:59 ./ti_cgt_c6000_7.4.5_setup_linux_x86.bin
ls -ld /tmp
drwxr-xr-x 20 root root 540 Oct 9 17:24 /tmp
ls -ld /tmp/ijtmp_46FB1DF1-FBD2-1937-F732-94959FF1F5B7/
drwxr-xr-x 2 root root 100 Oct 9 17:08 /tmp/ijtmp_46FB1DF1-FBD2-1937-F732-94959FF1F5B7/