I added the predefined symbols as I read was necessary for the uartstdio.c
ccs="ccs"
PART_TM4C123GH6PM
TARGET_IS_BLIZZARD_RA1
Whether I have these in there or not I get the following error log:
**** Build of configuration Debug ****
"C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all 
'Building file: ../main.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv5/tools/compiler/arm_5.1.1/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/TivaWare_C_Series-1.1" --include_path="C:/ti/TivaWare_C_Series-1.1/driverlib" --include_path="C:/ti/TivaWare_C_Series-1.1/utils" --include_path="C:/ti/ccsv5/tools/compiler/arm_5.1.1/include" -g --define=ccs="ccs" --define=TARGET_IS_BLIZZARD_RA1 --define=PART_TM4C123GH6PM --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp"  "../main.c"
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 135: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 135: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 136: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 137: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 137: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 137: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 138: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 138: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 139: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 140: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 140: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 140: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 141: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 141: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 142: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 142: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 143: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 143: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 144: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 144: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 145: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 145: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 146: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 146: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 147: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 147: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 147: error #20: identifier "bool" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 148: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 148: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 149: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 150: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 151: error #20: identifier "int32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 151: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 151: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 152: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 152: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 152: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 153: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 154: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 154: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 155: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 155: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 156: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 156: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 157: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 157: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 158: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 158: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 159: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 159: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 160: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 160: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 161: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 161: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 162: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 162: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 163: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 163: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 164: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 164: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 165: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 165: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 166: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 166: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 167: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 167: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 168: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 168: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 169: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 169: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 170: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 170: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 171: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 171: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 172: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 172: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 173: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 173: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 174: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 174: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 175: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 175: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 176: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 176: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 177: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 177: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 178: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 178: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 179: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/gpio.h", line 179: error #20: identifier "uint8_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 471: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 472: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 473: error #20: identifier "bool" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 473: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 474: error #20: identifier "bool" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 474: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 475: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 476: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 477: error #20: identifier "uint32_t" is undefined
"C:/ti/TivaWare_C_Series-1.1/driverlib/sysctl.h", line 478: error #20: identifier "uint32_t" is undefined
>> Compilation failure
Error limit reached.
100 errors detected in the compilation of "../main.c".
Compilation terminated.
gmake: *** [main.obj] Error 1
'Building file: C:/ti/TivaWare_C_Series-1.1/utils/uartstdio.c'
'Invoking: ARM Compiler'
"C:/ti/ccsv5/tools/compiler/arm_5.1.1/bin/armcl" -mv7M4 --code_state=16 --float_support=FPv4SPD16 --abi=eabi -me --include_path="C:/ti/TivaWare_C_Series-1.1" --include_path="C:/ti/TivaWare_C_Series-1.1/driverlib" --include_path="C:/ti/TivaWare_C_Series-1.1/utils" --include_path="C:/ti/ccsv5/tools/compiler/arm_5.1.1/include" -g --define=ccs="ccs" --define=TARGET_IS_BLIZZARD_RA1 --define=PART_TM4C123GH6PM --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="uartstdio.pp"  "C:/ti/TivaWare_C_Series-1.1/utils/uartstdio.c"
'Finished building: C:/ti/TivaWare_C_Series-1.1/utils/uartstdio.c'
' '
gmake: Target `all' not remade because of errors.
**** Build Finished ****
driverlib/gpio.h is not found in the directory it is looking for it at but not sure why it is looking for it in that specific directory. Any suggestions would be appreciated.