This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Upgrade failure from 5.3 to 5.5



Several errors reported when upgrading. Zipped InstallJammer log file attached. Urgent - have to go into hospital next week and must finish development! Thanks.

60556FE5-C1A1-4061-8DF8-FFB8393BAE2D.zip
  • Do not upgrade. Remove all old files and do a clean install.

    Regards,
    Maciej 

  • Two of the components failed to install. Could you attach the contents of this folder as well: C:/ti/ccsv5/install_logs

    You can manually update these two components as follows into your existing install.

    Download and extract this file: http://software-dl.ti.com/ccs/non-esd/scratchpad/dsemu.zip

    Exit CCS if running. Run the two installers. Enter an installation path of: c:/ti/ccsv5 for each.  The file contains the two components that failed to install. If they fail to install again when manually run, please provide the new logs created in C:/ti/ccsv5/install_logs and any other information on the error messages seen.