This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DSPBIOS for DSK5416 in CCSv5

Other Parts Discussed in Thread: PCM3002

Hello!

Can I create a DSP/BIOS Configuration File for the dsk5416 in CCSv5 in order to run the project "tone"

which is an example which come with CCSV3.1 ?

If yes how can I do it ?

If NO how can I run this project  in CCSv5 ?

I essentially need to generate file configuration for the Mcbsp2 and the PCM3002 Codec in order to

read and write data (16 bit)