Other Parts Discussed in Thread: UNIFLASH, CC2538
There appears to be bugs in the UniFlash platform on Ubuntu when dealing with CC2538 on SmartRF06.
1. UniFlash installed ok no errors although I had to adjust permissions on the Desktop Link to get it to work.
2. Create CCXML File operated without error creating a ccxml file for the CC2538SF53 and XDS100V3 combination.
3. Added a Program File and then tried to Program the CC2538. ERROR!:
Error connecting to the target:
(Error -233 @ 0x0)
The JTAG IR and DR scan-paths cannot circulate bits, they may be broken.
An attempt to scan the JTAG scan-path has failed.
The target's JTAG scan-path appears to be broken
with a stuck-at-ones or stuck-at-zero fault.
(Emulation package 5.1.73.0)
The Board and emulator is connected and recognised by the system
This needs an official fix asap