This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CSS V5.5 installation issue

Installating fails with a message to zip and send this folder to this forum.

I already have a 5.3 but wanted to update to v5.5.

Earlier I was getting the same error for v5.4 also

regards

Ashish

60556FE5-C1A1-4061-8DF8-FFB8393BAE2D.rar
  • Check by installing CCS v5.5 in a new folder say C:\tinew. 

    Also run the setup.exe file by right clicking on the exe file and click on "Run as Administrator"

    Hope this helps.

    Regards,

    Gautam

  • Installation of the Black Hawk emulation drivers failed. The log does not have details of what the specific Black Hawk issue was. There are a couple of options. You can find the Black Hawk installation logs in C:\Program Files (x86)\InstallJammer Registry\bh_emupack. If you post them here we will see what additional information there is. We could also try to run the BH installer by itself to see what additional feedback it provides. I'd like to first look at the log though.