Other Parts Discussed in Thread: TMS320C6748
6711 DSK with ccs 2.00 version.
First strange is, that product install just C6000 dsplib. C6700 dsplib not installed even if sale with 6711 DSK and 6711 DSK connected. Looks like 6700 (floating point) dsplib not in installation disk!
Ok then help sprc121. That additional contain 6700 (floating point) dsplib. After installation and linking to code I got error which originated from lib incompatibility.
Therefore need to relink library from soruce (because the oringinal one linked with other version). But cgtools (mk6x) cannot ass/link 67xx instruction even if sale with 6711 DSK and 6711 DSK connected (-mv6700 option ignored).
Therefore (that version of) DSK6711 demonstrate how DSK6711 not demonstrate capability of loating point C6xxxx DSP. Moreover that kind of CCS has no update possibility.
I welcome any idea...