This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linker warning: no matching section

Greetings Aarti!

I am doing precisely the same thing that Yaoxin was doing and succeeded, but I continue to see the following problem, when I build the project:

line 30: warning #10068-D: no matching section

line 31: warning #10068-D: no matching section

I am using CCS version:  5.4.0.00091

Would you kindly advice...thanks, Krishna 

 

  • Hi Krishna,

    I created a new thread for your question since the other one that you added the post to was really old and there is a good chance of those getting missed.

    Could you send me the full output from the CCS build console (you can copy build log to a file and attach it here)? Also if could attach your linker command file that would be helpful as well to understand where/why the warning may be appearing.